STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1429 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 560 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Dual core debugging: Is it possible to have a dual core debugging of the new STM32H7xx series using the STM32CubeIDE?

I've been trying to use the STM32CubeIDE together with a STM32H747-DISC0 board but I don't see a way to debug both MCU's at the same time. I can flash and debug each of the MCU's, but not both in the same time.Is there a way to do that? If not, is th...

LPers by Associate II
  • 733 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE and ubuntu 18.04 bash script

Hello, I use STM32CubeIDE on ubuntu 18.04.1 with the X-CUBE-AWS package and B-L475E-IOT01A board, during building process, postscript.sh script is invoqued to create bin file, but an error throw :"../../../../../BootLoader_OSC/2_Images_SECoreBin/SW4S...

When the "download" button available in the STM32CUBEIDE?

Hi, I find that there is no "download" button in the stm32cubeide. If users want to download the codes which generated by stm32cubeide(stm32cubemx), they must click the "debug" button first, then the software goto the UI of debug, and then the code d...

0690X00000BvscWQAR.jpg 0690X00000BvscbQAB.jpg
FLast.2 by Associate II
  • 1764 Views
  • 2 replies
  • 1 kudos

How can I burn an STM project into the STMF767ZI

1) How can I burn an STM project into the STMF767ZI in the STMCUBEIDE32 after I build the project?2) The Debug isn't working:STMicroelectronics ST-LINK GDB server. Version 5.2.3Copyright (c) 2019, STMicroelectronics. All rights reserved.Starting ser...

YShem.1 by Associate
  • 949 Views
  • 1 replies
  • 0 kudos

STM32CubeIDE Editor : Can't Type Tilda ~

STM32CubeIDE Version 1.2.1 in the editor I Can't Type Tilda ~ . I can type it in here ~I can type it in notpead, Word, all other places but not in CubeIDE editor. I'm using Turkish Q standart keyboard.

TŞEN.1 by Associate II
  • 2573 Views
  • 4 replies
  • 0 kudos