STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Linking error when adding Video Widget

Hello,I've followed the Generator User Guide to implement the Video decoding.Unfortunatly, when I add the video widget and try to run on target, I obtain the following error : Linking CM7/TouchGFX/build/bin/target.elf CM7/TouchGFX/build/River...

TLaur.3 by Associate II
  • 2455 Views
  • 4 replies
  • 0 kudos

Resolved! Images are distorted when the binaries are flashed from STM32CubeProgrammer, but works fine when flashed through TouchGFX ->Run target

Images used in the screens when TouchGFx project is created displays fine when the Binaries are loaded from TouchGFX ->Run Target. When the corresponding code generated for STM32cubeIDE is built and loaded on the board using STM32CubeProgrammer using...

KNara.2 by Associate III
  • 3198 Views
  • 6 replies
  • 0 kudos

Does the DBANK bit should be activated while using firmware on one bank or firmware size over 256 KB ?

Hi everyone,I have some misunderstanding about the use of the DBANK bit of the configuration bits.I have a costomized SPI bootloader located at address 0x0800 0000 and an Application starting at 0x08005000. So both are located on the Bank1. I made th...

MAmem.1 by Associate III
  • 3815 Views
  • 8 replies
  • 1 kudos

Resolved! Dynamic graph Y min and max labels.

Hi! I have a dynamic graph that I want to autoscale depending on max and min of the curve. So each time I get a new value I redraw the graph with the new Y range. I also want my graph to have two Y Axis labels: min and max. How do I achieve that? For...

MNema.1 by Associate III
  • 2796 Views
  • 4 replies
  • 0 kudos

RGB888 vs RGB565 Display type configuration in CubeMX

Am working on STM32H745BIT6 device with 16bit external SDRAM, 800x480 resolution RGB parallel TFT-LCD. On the Hardware all 24 RGB lines are connected to LCD.and LCD also supports 24 RGB. Plan to use TouchGFX for developing application.For using 565 c...

ATank.1 by Associate III
  • 6472 Views
  • 2 replies
  • 0 kudos