STM32 MCUs TouchGFX and GUI

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Error: Should never convert Action

Hi,After deleting some actions from a project I get this error:Sorry - something unexpected has happened which caused an error to occur in the Designer.For more information, see the log file located at: C:\Users\admin\AppData\Roaming\TouchGFX-4.23.2\...

codebuk by Associate II
  • 105 Views
  • 2 replies
  • 1 kudos

Upgrading TouchGFX engine and external buttons

This is an outstanding issue that's been there for a while but since it just got me again, I'm finally taking the time to post about it.  When using external buttons and the button controller, the implementation instructions have you edit the ToughGF...

Jazman by Associate III
  • 259 Views
  • 3 replies
  • 0 kudos

Resolved! Hard fault issue with octospi and touchgfx

Hello,I am working on a project that uses a STM32H7B3I-DK Board and an octospi memory MX25LM51245G. I also use the touchgfx library for the graphical interface.I encountered a hard fault issue that occurs randomly during the initialization of touchgf...