Does the DBANK bit should be activated while using firmware on one bank or firmware size over 256 KB ?
Hi everyone,I have some misunderstanding about the use of the DBANK bit of the configuration bits.I have a costomized SPI bootloader located at address 0x0800 0000 and an Application starting at 0x08005000. So both are located on the Bank1. I made th...