STM32 MCUs TouchGFX and GUI

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

TouchGFX absolute minimal sized build

I want to implement a bare bones TouchGFX bootloader application that provides text based feedback for status & %programmed. The idea is for the bootloader to be in FLASH sector0 and for it to be able to program a more complex TouchGFX based applicat...

dave2012 by Associate III
  • 265 Views
  • 0 replies
  • 0 kudos

Resolved! TouchGFX: How to enable an external data reader?

I am implementing a low cost custom TouchGFX project using a stm342G071 and an ILI9488 based display. For the ILI9488 driver I need the touchGFX framebuffer in RGB888 format.This works ok if I keep the image data in internal flash but I need to put ...

TMack.1 by Associate II
  • 554 Views
  • 1 replies
  • 0 kudos