User Activity

Hello,I'm trying to create a test application based on the SubGHz_Phy_Per RX example that will go into stop mode after initialization and wake up on EXTI line for an Rx window and then go back to stop mode.I want to base my test application on the Se...
I upgrade to 4.20 from a previous upgrade I did to 4.19.1 and I have those linker error:C:\Projects\projextx\Middlewares\ST\touchgfx\lib\core\cortex_m4f\gcc\libtouchgfx-float-abi-hard.a(PainterRGB565.o): in function `touchgfx::PainterRGB565::paint(un...
I'm using FreeRTOS in an STM32WL55 based application that needs to be active only few time per day (3-6).The system need to be in stop mode for most of the time and I have an external line that is connected to the LPTIM and based on this line status ...
I'm working in an environment with multiple targets and ST-Links.In previous versions of CubeProgrammer I had no problem to connect to a target with serial number X while other targets that are connected with other ST-Link are connect to the debugger...
Hello,I'm working with CubeMX 6.2 & CubeIDE 1.6.0.I have several problems with the generated code that I would like to know if I can somehow resolve instead of changing the generated code every time after changing something in the CubeMX project.This...
Kudos from