STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Will STemWin work with DMA for rotated screen ?

Hi,We are working with STM32F4 MCU and the Sitronix ST7789V (graphic driver) for a TFT display. We plan to use the STemWin library, however we need to rotate the screen. To reduce the footprint of the STemWin module, we will use the DMA of the MCU to...

is dcmi from stm32L4 compatible with stm32L4+ ?

Is there a difference in the usage of the DCMI peripheral between the l4 (STM32L49x) microcontrollers and the l4+ (STM32L4R5xx) chips? I have a camera working with dma on dcmi with the STM32L496, but the same c code does not work correctly with STM32...

stan_av by Associate II
  • 1349 Views
  • 2 replies
  • 0 kudos

DCMI to SD card with DMA on STM32H7

Greetings, Is it possible to 'stream' camera image data from DCMI peripheral to the SD card with DMA without using any intermediate external memory? This will reduce the need for another chip. Also would hardware JPEG encoding be possible in real tim...

PNare by Associate III
  • 1429 Views
  • 1 replies
  • 0 kudos

Is there any Documentation/Example of configuring the STM32F469i-Disco LCD with STemWin in STM32CubeMX?

I'm trying to generate a STM32CubeMX Project for AC6 but can't find the information necessary to do so. I tried to use the “default mode�?, look for the information inside the (working) BSP code and searched the web for the information or a preconfig...

STM32L4R5ZI is hitting "HardFault_Handler" after

Hello,I am using the stm32L4R5ZI Nucleo board with a MT9V024 camera sensor and a USB drive.I am using the HAL/STM32cubeMX library for the DCMI functionality using 10-bit parallel data with HSync and VSync as well (13 wires with 10-bit+Vsync+Hsync+DCM...

KM.8 by Associate III
  • 4279 Views
  • 5 replies
  • 0 kudos