STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

RGB888 vs RGB565 Display type configuration in CubeMX

Am working on STM32H745BIT6 device with 16bit external SDRAM, 800x480 resolution RGB parallel TFT-LCD. On the Hardware all 24 RGB lines are connected to LCD.and LCD also supports 24 RGB. Plan to use TouchGFX for developing application.For using 565 c...

ATank.1 by Associate III
  • 6485 Views
  • 2 replies
  • 0 kudos

Resolved! Bug when generating projet for STM32 with TouchGFX

HelloI'm working on a F412G-Disco board, with a TouchGFX application. When generating the initialisation code with MX, in the Core inc directory, MX generate a nema_hal.c fileIt contain only a file header. So, this is not a big problem but it is ann...

ANauz.1 by Senior II
  • 3412 Views
  • 7 replies
  • 0 kudos

How to get keypad input as hex

Hello everyone.​I Tried shared widget keypad with numbers. My question is how can get to hex from wildcard Unicode::UnicodeChar. Idea is to send simple CANBus message where is 9 wildcard input buffers and after char input it saves chars to a gui and ...

GunGo by Associate
  • 1901 Views
  • 2 replies
  • 1 kudos

STM32F469I-Discovery TouchGFX not working

Hello,i need to setup a TouchGFX project for STM32F469i-Discovery.I tried to create the project via STMCubeIDE with the TouchGFX Software Package.But the Screen remains black.I created the project in following steps:Create Project from STMCubeIDE v. ...

LDini.1 by Associate II
  • 6912 Views
  • 16 replies
  • 0 kudos

STM32 plus SSD1306. The project builds ok but display failed to work. When I go into debug I can step through all the code except the three functions from the display library I inserted in main.c . Init, Fill and Update. It jumps over them. Why?

< /* Initialize all configured peripherals */ MX_GPIO_Init(); MX_I2C1_Init(); /* USER CODE BEGIN 2 */ void ssd1306_Init(void); void ssd1306_Fill(White); void ssd1306_UpdateScreen(void);  /* USER CODE END 2 */ /* Infinite loop */ /* USER CODE BEGIN WH...

mseil.1 by Associate
  • 1133 Views
  • 0 replies
  • 0 kudos

USART1 and dynamic graph

Hi, I want to receive 20 bytes.I want to receive them every 2 milliseconds and simultaneously.To show data, I am working with TOUCHGFX. I use dynamic graphs to show them.The problem is, I want to show 12 bits on each graph.I debugged my code , it sea...

nsabo.1 by Associate II
  • 2993 Views
  • 5 replies
  • 0 kudos