STM32 MCUs TouchGFX and GUI

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32F746G-Disco Board // TouchGFX // DAC Issue

I have created a simple TouchGFX GUI on my STM32F746G-Disco Board. Everything works well. In my project I need a DAC . So I switched on DAC1 in CubeMX. But when I do so and flashing the code to the Board the screen do not show the genereated UI anymo...

UWall.2 by Associate
  • 526 Views
  • 3 replies
  • 0 kudos

DAC not working with TouchGFX

Hi, i'm working on a project where TouchGFX is running, but when i call the DAC via a FreerTOS task, nothing shows up in the output...Hardware wise everything is ok, tested baremetal and with a single FReertos Task, so TouchGFX or some interrupts mi...