STM32 MCUs TouchGFX and GUI

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32H745I-Disco crash at SystemClock_Config

I have a STM32H745I-Disco board which is still not supported. If I use an STM32H750B-DK example from TouchGFX (same board except mcu) I can download it from the designer and run it on the board. When I move the code to CubeIDE I can compile and downl...

hansd56 by Senior II
  • 1123 Views
  • 9 replies
  • 0 kudos

Resolved! Change Clock Source STM32F429i discovery

Hello everyone!I'm working on a TouchGFX project on an STM32F429i discovery boardWhen creating project automatically, the default clock source selected in my project is HSE clock source with HCLK frequency of 168Mhz, the program works fine. But when ...

TTú.1 by Associate III
  • 527 Views
  • 4 replies
  • 0 kudos

Resolved! HAL bug in glass LCD clock init (STM32L0)

in software package STM32L0 1.12.1in file stm32l0xx_hal_rcc_ex.cin functionHAL_StatusTypeDef HAL_RCCEx_PeriphCLKConfig(RCC_PeriphCLKInitTypeDef *PeriphClkInit)The RTC and LCD have their own settings, though they share the same clock.These settings a...

SZano by Associate III
  • 300 Views
  • 1 replies
  • 1 kudos

STM32G071 touchgfx example

Hello, I am generating a project from touchgfx with X-NUCLEO-GFX01M1. I manage to flash the board and make a basic example.However, when i move to CubeIDE, i am facing issues. First of all, i have added the external loader MX25L64.. to the debug. Aft...

0693W000008wvJIQAY.png
BHure.1 by Associate III
  • 377 Views
  • 3 replies
  • 0 kudos

STM32H735G-DK with HSI clock source

Hello,I am trying to reconfigure my STM32H735G-DK to use HSI instead of HSE for a TouchGFX based application.The Default config (at a high level):HSE Source, main CPU at 550 MHz and peripheral bus at 275 MHz or 137.5 MHz; OSPI at 200 MHz and LTDC at ...

RReta.1 by Associate III
  • 203 Views
  • 0 replies
  • 0 kudos