Resolved! will stemwin add gpu2d support ?
I cant use touchgfx well ,not familiar with c++.will stemwin add gpu2d support ?
I cant use touchgfx well ,not familiar with c++.will stemwin add gpu2d support ?
Hi,I am trying to implement STemWin v5.22 for an F4 MCU. I made sure to provide a path to the static library and included all the other necessary files. However I still get this error:../Lib\lib_STemWin522_CM4_GCC.a(GUI_Core.o): In function `GUI__Con...
Hi,after reviewing answers to following posthttps://community.st.com/t5/stm32-mcus-touchgfx-and-gui/how-to-draw-pixel-line-or-rectangle/td-p/105737and as a TouchGFX newby, I'm wondering: how one expects to do a following task by using TouchGFX's:ther...
As sure many of you know, the actual STM32H747i-disco can with a different display, so dont work with the examples in the 11.0 repository. But work perfect in the 11.1 if you set in the stm32h747i_discovery_conf.h /* LCD controllers defines */ #def...
Posted on August 17, 2017 at 18:07Hello all,I'm using the STM32F429 Discovery Kit and running the LTDC in 8 BPP (L8) mode. I have STemWin and am displaying their colour bar sample. I have a problem with colour conversion where the colour bars appear...
Hi everybody,I'm developing a simple gui on an STM32F429 microcontroller with the use of the STemWin grapich library. Everything is working well till I'm using just one framebuffer; now I would like to use double buffering to optimize the interface a...
Hello!Im having some problems with STM32F429ZIT about the interrupt handler. My microcontroller is connected on a LCD display by LTCD bus pheripheral and also has a interrupt input pin (PG2 - EXTI2 on falling edge detection border) connected on a ext...
Hi,I would like to try the hello world program from Stem win on my discovery board. Stem Win is not supported in STM cube ideCan anyone tell me how to proceed further to create and implement the project.Which IDE should I use.
Hello STM Community,I am currently working on integrating a third party SDK(blockchain sdk) with my FreeRTOS-based project on an STM32 microcontroller, and I have encountered a series of linking errors that I'm struggling to resolve. The build proces...
I’ve already asked and didn’t get any answer to the following question: how did it happen that TouchGFX, being ST product, does not support the very basic HW feature of each and every LTDC interface in STM32 controllers, namely – L8 (8bpp) format wit...