User Activity

Hi Community,How to store Video (.obj and .bin) files in external memory as they have stored in any generated project from Touch GFX designer?Already we stored image data in external memory by using pragma location and linker script. But now I want t...
I have integrated ILI9341 SPI display to Touch GFX. Frame Buffer Pixel Format is - RGB565 and getting the output. But when I change Frame Buffer Pixel Format from RGB565 to GRAY4 not getting the output.(Actually ILI9341 Supports RGB565). Is this poss...
Hi Community,I have followed the following link https://www.youtube.com/watch?v=suMytEyQTP4&t=774s and got the output (SPI display interfacing with Touch GFX). Now I wanted to use the single framebuffer strategy to get the same but no output. So, an...