STM32 MCUs TouchGFX and GUI

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H7 with TouchGFX __libc_init_array hardfault

Hi, i'm using STM32H750VB and it has 128kB embedded flash, so i'm using an external 16MB qspi flash. When i'm trying to fit firmware to internal & external flash, i modified linker script like this: base hal libraries are located in internal flash an...

Eralp by Associate III
  • 863 Views
  • 8 replies
  • 0 kudos

Resolved! stm32cubeide debug question

im debugging an LTDC project for the stm32f429zit6 on the disc board and in the sfr tab under rcc apb2enr it stops at tim11 and doesnt show ltdcen why is that and it seems my configurations in the ltdc registers arnt being set . im looking in the .sv...

Resolved! Hardfault getText() when debugging

For writing to QSPI flash, I suspend the touchgfx thread. In debugging mode, I get sometimes a hard fault. I thought it comes from switching from and to memory mapped mode of the QSPI, but now I think the problem is somewhere else. The fault occurs a...

awiernie by Senior II
  • 333 Views
  • 1 replies
  • 0 kudos