STM32 MCUs TouchGFX and GUI

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L073 about LCD Set-up Convertor when setting LCD_VOLTAGESORCE_INTERNAL. The set voltage and measured voltage are different.

Hello Developper Teams.​I use STM32L073.​About LCD Setting, The set voltage and measured voltage are different.​For example,  hlcd.Init.Contrast = LCD_CONTRASTLEVEL_0(2.6V) --> Measured voltage = 3.7VIs there another place to set it?​Setting HD=1 dro...

R.K by Associate II
  • 182 Views
  • 1 replies
  • 0 kudos

STM32 STOP mode with LCD

In an aplication using STM32L0 I need to enter the STOP mode when I realize the AC mains disappears and the uC must be powered by a battery.So before entering the STOP I obvioulsy deinit all the peripherals used till then and put the pins in analog m...

MVill.6 by Associate II
  • 435 Views
  • 4 replies
  • 0 kudos

Multiplexed drive of LCD

I have a custom lcd to drive with STM32L073VBTx's internal lcd driver. Duty cyle is 1/4 and the bias is 1/3. The problem is the common pins are activated sequentially even the LCD's RAM registers are equal to 0. When I activate some bits in LCD's RAM...

MCevik by Associate II
  • 409 Views
  • 5 replies
  • 0 kudos