MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! LIS3MDL calibration issues

I'm using a LIS3MDL magnetometer on my board, and I figured out how to calibrate it to account for distortions  caused by the board, and the procedure works. However, it seems that every time the same magnetometer is turned off and re-powered, the me...

bu by Associate
  • 174 Views
  • 1 replies
  • 0 kudos

Resolved! ST1VAFE3BX vAFE validation against reference signals

I'd like to validate ST1VAFE3BX vAFE measurement data against test signals as part of hardware design validation of a custom ECG sensor design based on ST1VAFE3BX. I intend to input reference signals (differential or single ended) into the two bio ch...

bwilkins by Associate II
  • 739 Views
  • 6 replies
  • 0 kudos

ISS2MDC High Power Consumption on Idle

Hello,I am evaluating the STMicroelectronics IIS2MDC magnetometer and measuring its supply current using a Joulescope. According to the datasheet, the device should draw approximately ~1.5 µA in idle mode, yet I consistently measure about 450 µA, whi...

LIS2MDL (LGA-12L) Leakage current

Hi Team,We have designed and manufactured several thousand PCBs that include the LIS2MDL (LGA‑12L) sensor. All boards are functioning correctly from an operational standpoint. However, because our devices run on battery power, load current is critica...

Mallik18 by Associate II
  • 515 Views
  • 8 replies
  • 2 kudos

Microphone self noise IMP34DT05

Hello,I'm using the IMP34DT05 microphone and it records fine but there is always a noise overlapped and it is very annoying.I have tried recording the background noise in anechoic chamber (see attached audio, high-pass filter alpha is 0.98). Do you k...

frnt by Senior
  • 2295 Views
  • 3 replies
  • 0 kudos

Resolved! I2C with IMS330dlc

Hi I am new to the I2C communications. I am trying to communicate to the IMS330dlc chip. I am using a lab jack U3-HV.. I am programming this via Visual Studio 2022 using c# code. I cant get back the 106 for Who am I. below is the code that I setup on...

Resolved! Clarification Request: LSM9DS1 On-Board Sensor Fusion

Hi all, I’m confirming whether the ST LSM9DS1 provides any on-board sensor fusion output (for example quaternion/Euler), or if fusion must be done on the host MCU. If anyone has definitive guidance from ST docs/support, please share. Thanks.