2026-03-12 11:51 AM
Hi everyone,
I am developing a custom board using an STM32U5 and the LSM6DSV16BX. I am using MEMS Studio to train and configure the Machine Learning Core (MLC), but I noticed that the generated .h configuration file seems to set INT1_MLC1 bit at MLC_INT1 register by default.
Even though I haven't explicitly set up physical pin routing in my project, the exported C array includes bank-switching logic that forces this configuration. I see the following sequence in my generated header:
{ .type = MEMS_CONF_OP_TYPE_WRITE, .address = 0x01, .data = 0x80 }, // Switch to Embedded Bank
// ... [other configs] ...
{ .type = MEMS_CONF_OP_TYPE_WRITE, .address = 0x0D, .data = 0x01 }, // MLC_INT1: Route MLC1 to INT1
// ... [other configs] ...
{ .type = MEMS_CONF_OP_TYPE_WRITE, .address = 0x01, .data = 0x00 }, // Return to Main Bank
Because of this, INT1 pin is firing on MLC state changes. Since this is a custom design, I need strict control over my interrupt routing.
My questions are:
Can someone confirm if routing the MLC to INT1 is indeed the default behavior of MEMS Studio?
If it is, is there an option or setting within the MEMS Studio GUI to change or disable this routing before exporting the .h file?
Thanks in advance for the help!
Best regards,
Rotem
Solved! Go to Solution.
2026-03-16 6:19 AM
Hi @RotemShechterN ,
Here our answers:
2026-03-16 6:19 AM
Hi @RotemShechterN ,
Here our answers: