MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Could you please explain me if the STM Android Sensor IIO HAL calibration tool is an external APK? And provide information about how could I enable and run the calibration_daemon?

Hello,We have been working with the LIS3DH Accelerometer on an Android 11 based device. We have Integrated the corresponding Kernel drivers and the STM Android Sensor IIO HAL.As per our understanding our Android device should be able to read values f...

EVazq.1 by Associate
  • 1765 Views
  • 4 replies
  • 0 kudos

LSM6DSV80X gyro offset

I am using the LSM6DSV80X to get roll-pitch-yaw from SFLP and gyro reading. I noticed that the sensor keeps reporting increasing yaw and increasing offset for X axis while at rest even though the data sheet suggests that it should have up to only 1dp...

qkieu_0-1756075772778.png
qkieu by Associate
  • 619 Views
  • 2 replies
  • 0 kudos

lsm6dsv320x WHO_AM_i

We're looking to use the lsm6dsv320x in our product. I'm using this senser on the on the STEVAL-MKI247A adapter board for testing. We're currently in development using the adapter board with the Nordic nRF52840DK board. I'm having issues with getting...

Screenshot 2025-07-03 114225.png
fk by Associate II
  • 1114 Views
  • 15 replies
  • 5 kudos

STHS34PF80 Presence and motion sensor

 Hello,        In my case, the STHS34PF80 sensor module is powered using I2C communication with the ESP32 module, and I have tested its functionality only up to 2 feet; beyond that, it fails to detect any presence. However, the datasheet indicates th...

Resolved! STATUS_REG of the ASM330LHH

How long does the TDA bit in the STATUS_REG of the ASM330LHH remain “1”?Is the TDA bit itself a latch type and remains “1” until the temperature output register (OUT_TEMP_H/L, 21h/20h) is read?

ggob by Associate III
  • 183 Views
  • 2 replies
  • 0 kudos

Resolved! ASM330LHH CTRL9_XL DEVICE_CONF

It is recommended that CTRL9_XL DEVICE_CONF in ASM330LHH always set this bit to 1 when configuring the device, but when should it be set back to 0? Should it not be set back?

ggob by Associate III
  • 632 Views
  • 2 replies
  • 0 kudos

Resolved! LSM6DS3 SPI Bug?

Hello, I use an AT32F403A MCU to connect LSM6DS3 IMU via SPI 4-wire, then I read the WHO_AM_I register at 0x0F. According to the datasheet, the return value should be 0x69, but the chip returned 0x44. Then I repowered the board, and the value seemed ...

Wakkk_0-1756302516517.png Wakkk_1-1756302521207.png Wakkk_2-1756302530679.png
Wakkk by Associate
  • 545 Views
  • 2 replies
  • 2 kudos