MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

data collection

How many data points are necessary to build a reliable machine learning model (with mlc)? Is there a point where adding more data no longer significantly improves the model's performance?

SamuPre by Associate II
  • 3170 Views
  • 1 replies
  • 0 kudos

st_lsm6dsvx: odr_calib seems wrong

Hello,I think there is two errors in the st_lsm6dsvx driver in the odr_calib calculation algo : odr_calib = (data * 37500) / 1000 :data should be casted in s8 like in other driversthe formula seems wrong according to the datasheet :Formula seems to u...

Resolved! Calculating THRESH1 for the FSM and ISM330BX accelerometer

I'm doing a 4D orientation detection FSM on the ISM330BX. There is no example for this IMU so I'm following the examples for some of the other IMUs. That is fine and the code works, but what I can't work out is how to calculate the THRESH1 value and ...

reefwing by Associate II
  • 2082 Views
  • 2 replies
  • 1 kudos

Simple Accelerometer Configuration

Posted on May 08, 2013 at 17:40 Hi, I'm trying to configure the accelerometer on my stm32f4 discovery board. I lost with all the configuration of LIS302DL and TIM4 (example code) and do I need to configure SPI1 separately??? I si...

vault by Associate
  • 1457 Views
  • 2 replies
  • 0 kudos

Resolved! I can't use MEMS-studio under KDE/Plasma (linux)

Hello,in KDE/plasma environment I can't use MEMS-studio because it doesn't show file dialogs.For example: MEMS-studio is connected to the STEVAL-MKI109V3 board, in "Advanced Features" -> "FSM" I click the "Load state machine from file“ button, but no...

zmogas by Associate II
  • 2788 Views
  • 5 replies
  • 2 kudos