MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Looking for Accelerometer

Hi, I am looking for an accelerometer. I wonder if there is any ST MEMS chip that meets my requirements:I don't need very high max G force: 4/8G should be enoughLow power consumptionAble to send trigger, like a GPIO rising or falling signal, when acc...

HDaji.1 by Senior
  • 695 Views
  • 1 replies
  • 0 kudos

LSM6DSL big gyroscope fluctuations on acceleration

Hello, I am using a LSM6DSL sensor and when applying a 2G acceleration without rotating the board, I get very important spikes on the gyroscopes of about -90°/s to +90°/s amplitude.This is very strange. Is this a normal behaviour from this sensor ? A...

lsm9ds1-gyroscope

Hi,I have an application with LSM9DS1 sensor and I expected that when I change LSM9DS1 sensor position from horizontal to vertical value will change but changed only when sensor was moving but after that valus comes almost same for horizontal or vert...

JarekG by Associate
  • 830 Views
  • 1 replies
  • 0 kudos

Resolved! IMU Sensor Fusion Performance

Hi Team,I searched sensor fusion performance information of LSM9DS1TR, LSM6DSO IMUs as below,1. Static Accuracy (Yaw, Pitch, Roll) = ?2. Dynamic Accuracy (Yaw, Pitch, Roll) = ?3. Orientation Settling time = sec?However, I did not find it in the respe...

VB.4 by Associate II
  • 784 Views
  • 1 replies
  • 0 kudos

MEMS Studio Path: resample_odr.exe does not exist.

In MEMS Studio under advanced features > MLC I upload a data pattern and label it under the "Data Pattern" tab. On the "Datalog analysis" tab when I click the Run button it gives the following error.Path: resample_odr.exe does not exist. Please check...

LosKlong_0-1724496672445.png LosKlong_1-1724496895495.png
LosKlong by Associate
  • 776 Views
  • 1 replies
  • 0 kudos

Resolved! Sensortile in cradle is not working with microsd card

Hello all, I wanted to use sensortile to collect data on microsd card. (I have two of them) So, One portable cradle from the kit working good, but another is not working with the same microsd card. When start it from the android app the sensor just b...

Boris- by Associate
  • 1027 Views
  • 2 replies
  • 0 kudos

Resolved! Oddity in Meta-classifier in LIS2DUX12

Hello,the LIS2DUX12 documentation (AN5903: LIS2DUX12: machine learning core) contains a table explaining how meta-classifier works:At the third column from the end of the table, the decision tree gives the result "A".As far as I understand, the "B" c...

Ekrano kopija_20240809_140626.png
zmogas by Associate II
  • 930 Views
  • 1 replies
  • 0 kudos

Resolved! How config IIS3DWB to FIFO mode with Watermark?

Hi, I'm trying to use the IIS3DWB as FIFO mode with a watermark.I'm using a custom board. I double checked the hardware and guaranteed this board works well. I'm able to read/write the sensor using SPI interface and generate interrupt with wake-up in...

uilter by Senior
  • 1724 Views
  • 3 replies
  • 0 kudos

Resolved! Are LIS2DW12 registers non-volatile?

I want to setup the wakeup configuration registers and then disconnect the accelerometer from an I2C programmer and power source. When the accelerometer is placed with the new circuit, will the configurations in the register I have set still remain? ...

Lab1tr by Associate II
  • 872 Views
  • 3 replies
  • 0 kudos