MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Button with GPIO and Blueooth possible?

Posted on September 29, 2011 at 13:23Hi, my question is if it's possible to connect a button to the inemo v2 board which I need in an application as start button (or can i use one of the buttons on board, but how can I get the button status (presse...

DFU DLL's

Posted on August 29, 2011 at 12:35Does anybody have a source for the following DFU Dlls.Can ST support for the sameSTDFU.dllSTDFUFiles.dllSTDFUPRT.dllAlso has anyone used the above dlls provided by ST to create their own DFU application on PC. We ar...

royston by Associate II
  • 737 Views
  • 1 replies
  • 0 kudos

Sample codes to program with iNemo V2 SDK

Posted on September 16, 2011 at 12:55Hi all, I would like to know where can I find the sample codes to work with iNemo V2 SDK. The sample project that comes with the installation is so simple. Are there any further available sample codes to download...

pnhoang by Associate
  • 605 Views
  • 1 replies
  • 0 kudos

Tap detection

Posted on September 08, 2011 at 16:49Hi,    I am trying to do double tap detection at 10hz and 25hz .Is this possible at low frequency. Viewing the acceleration graphs in Inemo PC suite I could see that the response is poor at low frequency and good...

1.8v Digital Power supply for accelerometer

Posted on April 09, 2011 at 20:49Hi,   Could someone tell me what is the reason for having a 1.8V supply for the digital I/O of the accelerometer.One reason Im guessing could be lower power consumption and compatibility with lower voltage peripheral...

Inemo Dfuse problem

Posted on August 12, 2011 at 10:23Hi,    I am currently developing a PC application for STM32 using Inemo board.The PC application will be able to upgrade the firmware of the STM32 using Dfu mode. Iam using Visual studio Vb.net for the PC side appli...

How can I write to the SD card

Posted on August 08, 2011 at 23:47Hi all.Sorry for the simple question, but I'm totally new to this but how can I write the sensor output to the SD card? I can't seem to find info on it in the documentation.My intention for using the board is for Da...

gummih by Associate
  • 1049 Views
  • 1 replies
  • 0 kudos

iNEMO V2 alignment with 3D cube for perfect rotation

Posted on August 04, 2011 at 09:27HiCould anyone tell  how to align iNEMO V2 Board with 3D Cube (on monitor) to see the perfect rotation. ST provides a small 3D Cube demo, it's ok. I want to the in my VC++ program to accomplish the same alignment.1....

harinath by Associate III
  • 651 Views
  • 0 replies
  • 0 kudos

Download software on the board without debugging

Posted on July 28, 2011 at 12:35Hello, After downloading my software on the board, it only can executes when I am in debugging mode and make a RUN. When I restart the board without debug, my software isn't effective anymore, whereas it's supposed t...