cancel
Showing results for 
Search instead for 
Did you mean: 

Button with GPIO and Blueooth possible?

sam239955
Associate II
Posted on September 29, 2011 at 13:23

Hi,

my question is if it's possible to connect a button to the inemo v2 board which I need in an application as start button (or can i use one of the buttons on board, but how can I get the button status (pressed = true/false) with the DLL?

other question is that I have a bluetooth module that uses i2c, can I connect it with the iNemo via the pin connectors? Is that possible?

regards

Alex
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0