MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

FIFO timing Error

Posted on December 20, 2011 at 20:27I am facing timing issue with lis3dh accelerometer in FIFO mode.Currently my ODR=25 Hz and I am reading FIFO on watermark threshold=30.As soon as I get watermark interrupt I read 196 (32*3*2)samples at 5 Mhz.Hence...

software problem iNEMOEngine LI3

Posted on January 17, 2012 at 08:02Hi ST-team,i have downloaded the iNEMOEngine LI3 software. After the registration I get the link to download the file with the name: ''iNEMO_Suite_2.3.0_110913.zip''. When I try to open it I get an error message th...

nikolaj by Associate
  • 555 Views
  • 1 replies
  • 0 kudos

STeval-MKI 109V1, also V2

Posted on December 29, 2011 at 11:04Hi,I intend to use several STeval-MKI109Vx structures, up to ten systems, simultaneously, andall of them ''wireless''. STM offers a wireless Bluetooth kit for connecting to STeval-MKI109V1.Is it possible to use up...

Ploblem with JLINK and iNemo broad

Posted on December 06, 2011 at 11:42Hi,I met this problem, iNemoand computerconnectionssuggested that ''could notdistinguish between USBdevices, '' First of all, I wanted to step through the code line by line with JLINK, under the RDI mode, But aft...

dxpfigo by Associate
  • 556 Views
  • 0 replies
  • 0 kudos

Problem with SD card interface on Inemo

Posted on August 16, 2011 at 14:32Hello,         Im facing a problem with the Inemo SDcard api. Iam able to read and write multiple blocks and single blocks but Im not able to erase the card. When I issue a command for erase and then read the block ...

Spruce -SolidDigi STM32 Arduino Compatible Board With LCD

Posted on November 02, 2011 at 10:25Spruce -SolidDigi STM32 Arduino Compatible Board With LCDSpruce -SolidDigi STM32 ARM cortex board can be used with http://www.cutedigi.com/product_info.php?products_id=4408 and is compatible with http://www.cutedi...

help getting inemo board working

Posted on October 17, 2011 at 15:55I received the mk1062v2 board today. Eventually go it working by upgrading software and firmware. However I cannot get the magnetometers to deliver any data. They flatline. Also of interest is that in raw data mode...

Can i use iNemo v2 firmware and AHRS code on iNmeo v1..

Posted on October 06, 2011 at 13:51Hi! I have iNemo V1. As St Microeletronics has released AHRS source code which is written for iNemo v2... can i use this source code on iNmeo v1 .. can i use the firmware in a SDK V2.3 on iNemo V1..  thanks Hunza...

how to use USR SW2 Button

Posted on September 29, 2011 at 15:09hi, how can I get the user button event over the wrapper.cs / SDK ? I need it for my application. regards Alex

sam239955 by Associate II
  • 1037 Views
  • 4 replies
  • 0 kudos