MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Can the ST BLE Sensors Mobile App be Customised?

Hi.I'm an intern working with the SensorTile.Box Pro for a project. As the subject suggests, I was wondering if the mobile app provided with the box could be modified, and if so, how?May sound like a dumb question, but I saw that the source code for ...

NeoWei by Associate II
  • 597 Views
  • 0 replies
  • 0 kudos

LIS2DW12 - Wake up with Tilt and Scale question

I'm using the LIS2DW12 accelerometer to detect and classify different types of vibrations. I need to configure a wake-up threshold for a specific scenario.Two questions:1. When the sensor is set to 2g and I use the WK_THS[5:0] configuration, setting ...

SPiy1_0-1723832020701.png
SPiy.1 by Associate
  • 720 Views
  • 1 replies
  • 0 kudos

MotionSP FFT q15 or q31 instead of float32

Hello Community,I am trying to implement a basic FFT computation on our STM32G0 MCUs using MotionSP for a 16-bit accelerometer signal.I am not sure why does MotionSP by default uses float32 for FFT when the original sensor signal is 16-bit?Can I then...

Chubs by Senior
  • 735 Views
  • 1 replies
  • 0 kudos

Resolved! LPS22 sensor

Hello,I'm trying to disable temperature compensation on the lps22hh sensor, does anyone know if there's a specific register i can manipulate? Thanks!

ILPS28QSW Gel Info

Hello all,I am looking for more info on the gel used with ILPS28QSW.We want to use it in an application where the sensor may be submerged in 10% to 40% alcohol v/v for extended periods of time. Will the sensor be okay? Or is there another product whi...