Question
Obsolescence of IIS328DQTR and equivalent components
Hey!
If I well understood the component IIS328DQTR will be at least "NRND" in 2025.
The IIS3DHHC seems to be a good substitute but it doesn't have all the interrupt features of the IIS328DQTR.
Can you confirm the lifetime of the IIS328DQTR?
Do you have a 3-axis digital accelerometer with the feature: "The device may be configured to generate an interrupt signal through inertial wakeup events, or by the position of the device itself."
Kind regards
Charles D