MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LIS331HH data rate

Posted on July 08, 2015 at 14:00Hello, does anybody know how accurate the data rate of the LIS331HH sensors should be? I use two with a data rate of 1000Hz of them and want to synchronize the measurment results. For this reason i measured the Interr...

bognermn by Associate
  • 484 Views
  • 0 replies
  • 0 kudos

Lsm9ds0 interrupt delay issue

Posted on July 06, 2015 at 14:49I am using Lsm9ds0 device connected to imx6 processor via i2c with following configuration. Set Gyro ORD to 95hz. Set Watermark level to 30 Set to Stream mode register configuration {CTRL_REG3_G, 0x04},     {CTRL_REG4...

sijilcv by Associate
  • 516 Views
  • 0 replies
  • 0 kudos

LSM303D Interrupt

Posted on July 06, 2015 at 09:06Hello,I am using Lsm303D, it works well but I am not lucky with the interrupt functions.Anybody helps me to give me a good sequence of sets to have an interrupt on INT1 or INT2 when my board is slightly shaken ?I have...

LIS2DH - suspected noise

Posted on July 02, 2015 at 14:53Hello there, I had placed the LIS2DH on my board , and it seems to work fine. using default setting and 10Hz sampling, when i am putting the PCBA on a fixed position, and X axis raw data is unstable from - 128 to 128....

nir23 by Associate
  • 499 Views
  • 0 replies
  • 0 kudos

Unable to get axis data on LIS2DHH

Posted on July 02, 2015 at 14:50Hey, I have to communicate with LIS2DHH , and dummy byte received fine, however when i am trying to read axis data i get only 0.

nir23 by Associate
  • 501 Views
  • 0 replies
  • 0 kudos

Did I just brick my evaluation board?

Posted on December 17, 2013 at 16:12Hello,I bought a STEVAL-MKI109v1  evaluation board, and a STEVAL-MKI114v1 probe about 1,5 years ago.Yesterday I tried to get it to work with the latest version of the Unico test software, but the program would alw...

joeri by Associate
  • 1075 Views
  • 2 replies
  • 0 kudos

Capacitance/Voltage Converter

Posted on June 24, 2015 at 19:36Hello all, I would like to use an off-the-shell CVC as readout for my capacitive MEMS accelerometer. My concern is the acceptable input bulk capacitance, that is 30pF in my case. I have looked in a couple of CVCs, MS...

AHRS continous problem under CoIDE

Posted on April 19, 2015 at 20:33 Hi to all, I'm trying to use this demo, and I have noticed that my program remains blocked at this line of the iNEMO_AHRS_Init() void iNEMO_AHRS_Init(iNEMO_SENSORDATA* pSensorData, iNEMO_EULER_ANGLES* pAngle,...

daniel23 by Associate II
  • 779 Views
  • 2 replies
  • 0 kudos

A terrible question when i use MP45DT02

Posted on August 16, 2014 at 06:03Hi,I am Jessenow,i will use MP45DT02 in my projectbut i evaluated it in STM32F407-DISCOVERY,i found a kind of terrible noise , it sounds like ''dot……dot……dot……'',especially female voice.wish a solutionthank you very...