cancel
Showing results for 
Search instead for 
Did you mean: 

A terrible question when i use MP45DT02

jianxiong_1009
Associate
Posted on August 16, 2014 at 06:03

Hi,I am Jesse

now,i will use MP45DT02 in my project

but i evaluated it in STM32F407-DISCOVERY,

i found a kind of terrible noise , it sounds like ''dot……dot……dot……'',especially female voice.

wish a solution

thank you very much

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
jianxiong_1009
Associate
Posted on August 22, 2014 at 11:45

I solved it. 

I increased the RAM of the AUDIO-BUFFER

excellent mems-microphone!!

this is the point:

 /* Defines for the Audio recording process */

  #define RAM_BUFFER_SIZE         8000  /* 3Kbytes (1500 x 16 bit) as a RAM buffer size.

                                           More the size is higher, the recorded quality is better */ 

f23
Associate II
Posted on June 09, 2015 at 19:20

Hi,

Can you show me your code if you dont mind. Do you used PDM filter for the signal processing?