MEMS (sensors)

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

DRIVER EXAMPLE FOR LSM330DLC

Posted on December 09, 2013 at 13:31Hello to all, In order to ease the self learning process and setup ST's LSM330DLC, attached to this post is an example of its drivers setup for a general application. Thank you, Thiago Reis #lsm330dlc

Drivers Examples for LSM303D

Posted on December 09, 2013 at 13:29Hello to all, In order to ease the self learning process and setup ST's LSM303D, attached to this post is an example of its drivers setup for a general application. Thank you, Thiago Reis #lsm303d

Driver Example for L3GD20

Posted on December 09, 2013 at 13:20Hello to all, In order to ease the self learning process and setup ST's L3GD20, attached to this post is an example of its drivers setup for a general application. Thank you, Thiago Reis

Setting up LIS2DH for 6D movement recognition

Posted on November 27, 2013 at 22:37I am trying to setup the LIS2DH to detect movement and drive INT1.  The documentation is not clear what needs to be configured to do this. CNTL_REG3 appears to select the sources for INT1.  There are two that are ...

mvonahnen by Associate III
  • 487 Views
  • 1 replies
  • 0 kudos

Data Ready Interrupt

Posted on November 27, 2013 at 14:38Hi, my INT1-Line is static low: with:     response = LIS331DLH_SetIntHighLow(MEMS_ENABLE);  // Interrupt active low; and     response = LIS331DLH_SetInt1DataSign(LIS331DLH_DATA_READY); I get the data only about p...

steffen by Associate II
  • 651 Views
  • 3 replies
  • 0 kudos

Access to the iNemo evaluation board firmware

Posted on August 09, 2013 at 23:45I have purchased the STEVAL-MKIO62v2 evaluation kit and I am looking for the source code so I can rebuild the firmware for this board.  Essentially I need the source code for the RTOS that goes on the MCU as well as...

LSM9DS0 Accuracy

Posted on November 02, 2013 at 05:06The LSM9DS0 datasheet only appears to mention the accuracy of the accelerometer!?!? So the gyro and magnetometer have no accuracy specification?  Please explain!!

MEMS Accel Eval Kit

Posted on October 14, 2013 at 15:04I have the STEVAL-MKI109V2 with the MKI135V1 accelerometer module.  I've installed the Unico eval software v3.0.0.0.  The COM port matches.  There are no errors.  I'm on Win7/64.There is no data.What am I missing?T...

dlasley by Associate II
  • 1101 Views
  • 7 replies
  • 0 kudos