cancel
Showing results for 
Search instead for 
Did you mean: 

Lsm9ds0 interrupt delay issue

sijilcv
Associate
Posted on July 06, 2015 at 14:49

I am using Lsm9ds0 device connected to imx6 processor via i2c with following configuration.

Set Gyro ORD to 95hz.

Set Watermark level to 30

Set to Stream mode

register configuration

{CTRL_REG3_G, 0x04},    

{CTRL_REG4_G, 0x20},    

{CTRL_REG5_G, 0x40},    

{CTRL_REG1_G, 0x0F},    

{FIFO_CTRL_REG_G, 0x5E},

I would expect a water mark interrupt at an interval of every 316ms(1/95*30). but I could see interrupt at an interval of every 340ms

Could you please help me to identify the delay in interrupt. The same behavior is observed in the case of accelerometer and magnetometer. Inside ISR the entire FIFO data is read in burst mode based on the FIFO status register.

#lsm9ds0
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0