Posted on April 19, 2015 at 20:33
Hi to all, I'm trying to use this demo, and I have noticed that my program remains blocked at this line of the iNEMO_AHRS_Init()
void iNEMO_AHRS_Init(iNEMO_SENSORDATA* pSensorData,
iNEMO_EULER_ANGLES* pAngle,...
Posted on April 15, 2015 at 19:50Hi to all, I'm trying to program my iNemo based custom board with the ST LINK provided with the STM32F4 Discovery. When I try to connect with STM32 ST-Link Utility I get the error: '' Core is held in reset''. Another...
Posted on April 12, 2015 at 21:12Hi, I have developed, printed and mounted a custom iNemo based board: I noticed a short circuit between Vcc and Gnd with my multimeter, so my question is: there is an hidden problem in my circuit (like a short circui...
Posted on April 11, 2015 at 22:49Hi to all, I have developed my own ST iNemo based board, and I'm trying to program it with the Discovery board. The iNemo board is connected to the VCC pin of the discovery for the power supply while programming, and...
Posted on March 25, 2014 at 11:19
Hi, I'm trying to compile (I have already done the config files) the library with my project, where are present all the include files of the library.
I have included the following options for the linker:
...
Posted on June 17, 2015 at 10:20 Yes, I have found a solution but I haven't updated this post sorry. I attach a PDF that is taken from my project report and briefly explains how to solve the problem. Daniel
________________
Attachment...
Posted on April 12, 2015 at 10:40 I have attached my schematic, using SWD connector linked to my Discovery board, and discovery linked to the pc through the USB connection, my boot0 pin has to be connected to gnd or left floating? My NRST is no...
Posted on February 14, 2014 at 20:55I'm trying to use emWin demo with stm32F4 Discovery and SS2119. Is there anyone can share the working demo with me? my email is: daniel.casini@gmail.comThanks,Daniel
Posted on February 14, 2014 at 20:47I'm using an LCD provided with the expansion ( http://www.element14.com/community/community/knode/dev_platforms_kits/element14_dev_kits/stm32f4-discovery-expansion-boards ) which uses SSD2119 as LCD controller.Sho...