MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LPS25HB pressure measurement in liquid environment

Posted on August 02, 2016 at 09:55Hi, For a solution we want to use the LPS25HB in a liquid environment. In our opinion, the best way to do this is by installing the sensor in an oil filled case with a thin metal membrane on the top. On this way the...

0690X00000603AsQAI.jpg

LSM303DLHC accelerometer output data is 15344.

Posted on July 26, 2016 at 06:19Should my program get 1000 mg when F3 Discovery Board is in steady state on a horizontal surface? Measurement range = [-2g;+2g]; Linear Axeleration Sensitivity = 1mg/LSB; High Resolution Mode I get 15344 mg (0x3BF0) a...

L3G4200D randomly boots with different zero-rate drift

Posted on April 22, 2015 at 09:20We use an L3G4200D rate-gyro in our project.Part of the setup involves acquiring calibration data from the sensor (zero-rate drift versus temperature as reported by the sensor itself).After applying the collected cal...

sales2 by Associate
  • 1488 Views
  • 1 replies
  • 0 kudos

lsm6ds3 SPI code

Posted on July 27, 2016 at 23:17Hello, We are using lsm6ds3 sensor by connecting to STM32F103 controller through I2C communication. Over I2C to read both X and G Raw data taking around 800uSeconds over 400K speed. In one of my new project, needed bo...

suresh by Associate II
  • 1524 Views
  • 1 replies
  • 0 kudos

Calculation Xh and Yh in eCompass

Posted on July 17, 2016 at 14:04Hello everyone, I can not understand how they obtained the equation 2 p. 7 the following document: Can anyone explain me? Thank you and greetings. #ecomapass-tilt-lsm303dlh #ecompass #tilt #lsm303dlh

torrepa by Associate
  • 1081 Views
  • 2 replies
  • 0 kudos

LPS22HB - One shot mode problem

Posted on July 16, 2016 at 21:04Hi, I try to get the pressure data in One shot mode. I read the state of Reg Who am I (0Fh)=B1h Ctrl_Reg1 (10h)=00h, Ctrl_Reg2 (11h) =10h, then I write to Ctrl_Reg2< 11h, to provide One Shot Mode, Now continuous read...

bvn123 by Associate II
  • 1703 Views
  • 3 replies
  • 0 kudos

STEVAL-MKI094V1

Posted on April 12, 2016 at 12:22Hi, I have recently acquired an STEVAL-MKI094V1 and can't find the software downloads for this board on the ST site.  Can anyone advise where I might find please.  I need either for Mac or PC, Mac preferred but PC wi...

ray2 by Associate
  • 831 Views
  • 1 replies
  • 0 kudos

wesu board drift

Posted on July 15, 2016 at 12:08Hello, I just received the wesu board and I using it ''as it is'' with the related android app ST WeSU. What I'm facing looking at the cube on the app is that there is a very high drift of the cube itself. In details:...

fabiano by Associate
  • 842 Views
  • 1 replies
  • 0 kudos

Using LSM9DS0 as a vibration sensor

Posted on June 28, 2016 at 17:56I'm trying to use LSM9DS0 as a vibration sensor using accelerometer data, but I have some questions regarding the datasheet:1. Do I need to have magnetometer activated in order to use 6D in INT_GEN_1_REG? If I don't a...

Question about X-NUCLEO-IKS01A1.

Posted on July 18, 2016 at 16:01 I have an X-NUCLEO-IKS01A1 board. There is a LSM6DS0 on the board but the following functions DrvStatusTypeDef BSP_ACCELERO_Enable_Free_Fall_Detection_Ext( void *handle ); DrvStatusTypeDef BSP_ACCELERO_Disable...