cancel
Showing results for 
Search instead for 
Did you mean: 

LSM303DLHC accelerometer output data is 15344.

daniil-denisov
Associate
Posted on July 26, 2016 at 06:19

Should my program get 1000 mg when F3 Discovery Board is in steady state on a horizontal surface?

Measurement range = [-2g;+2g];

Linear Axeleration Sensitivity = 1mg/LSB;

High Resolution Mode

I get 15344 mg (0x3BF0) and -16912 mg (0xBDFO) when the board is upside-down.
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Miroslav BATEK
ST Employee
Posted on August 01, 2016 at 18:35

The output of the accelerometer sensor is 12-bit left adjusted. You have to divide the sensor output value by 16, then you will get correct value in [mg] unit.

Best regards

Miroslav