MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Simple Accelerometer Configuration

Posted on May 08, 2013 at 17:40 Hi, I'm trying to configure the accelerometer on my stm32f4 discovery board. I lost with all the configuration of LIS302DL and TIM4 (example code) and do I need to configure SPI1 separately??? I si...

vault by Associate
  • 923 Views
  • 2 replies
  • 0 kudos

Resolved! I can't use MEMS-studio under KDE/Plasma (linux)

Hello,in KDE/plasma environment I can't use MEMS-studio because it doesn't show file dialogs.For example: MEMS-studio is connected to the STEVAL-MKI109V3 board, in "Advanced Features" -> "FSM" I click the "Load state machine from file“ button, but no...

zmogas by Associate II
  • 1358 Views
  • 5 replies
  • 2 kudos

Could you please explain me if the STM Android Sensor IIO HAL calibration tool is an external APK? And provide information about how could I enable and run the calibration_daemon?

Hello,We have been working with the LIS3DH Accelerometer on an Android 11 based device. We have Integrated the corresponding Kernel drivers and the STM Android Sensor IIO HAL.As per our understanding our Android device should be able to read values f...

EVazq.1 by Associate
  • 1794 Views
  • 3 replies
  • 0 kudos

Resolved! LIS2DH12 proper free-fall detection settings

Hi,I'm having trouble following how to properly setup free fall detection on the LIS2DH12. I'd like to generate an interrupt when the device goes from rest to free falling for a couple feet. The duration of the fall would be approximately 200ms. I'm ...

Resolved! MotionFX VS MotionDI lib for 6axes fusion

Hello,both of MotionFX 6X and MotionDI return the same output (rotation vector, quaternion, gravity, and linear acceleration)so what is the difference between theme, and witch one is more suitable for 6 axes fusion ?should i implement additional cali...

malarab by Senior II
  • 646 Views
  • 1 replies
  • 0 kudos