MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LIS3MDL single measurement mode

Posted on June 12, 2017 at 12:08Hello, I would like to use the LIS3MDL magnetometer in single measurement mode to reduce my overall current consumption.I've found some useful informations in the AN4602 Application but I'm still missing something.The...

LSM9Ds1 Self-test

Posted on January 12, 2016 at 13:15How may i know about self-test, what is the procedure after enable self-test for each one, and what kind of data will there that i have to use for further analysis, and how. #self-test

bhavesh by Associate II
  • 1257 Views
  • 4 replies
  • 0 kudos

lsm9ds1 self test

Posted on July 31, 2017 at 12:56Hello, I want to do a self test to lsm9ds1.Is there any file that explain how to do it?I found some sources  but nothing official.If there is not official file, i have some questions:Is the sensor can't be in motion a...

4D/6D threshold setting for LIS2DS12

Posted on July 07, 2017 at 02:25Dear sir/madam,I'm confused how the Threshold decodeing(degrees) comes like shown in LIS2DS12 datasheet, page 31. When 6 stands for 80 degrees and how 6 comes from?I try to use 60 degrees threshold and I can read accu...

0690X00000603kIQAQ.jpg

LIS3MDL_Interrupt problem

Posted on September 03, 2017 at 10:27Hello sir,HELLO EVERYBODY,I have a question about LIS3MDL.   Expecially, interrupt problem.I am using LIS3MDL below sequence.=================================================================================1. In ...

LIS2DH FIFO in SPI mode

Posted on July 13, 2017 at 14:06I did not quite understand from the pdf when reading 32*3 samples from the FIFO in SPI mode, can I set the SPI starting address at OUT_X_L (28h) with the SPI's MS bit raised and then read in a constant SPI read stream...

I am using LIS3MDL and is there any way to offset the interrupt threshold values by changing the Offset Registers? What I mean is suppose my surrounding environment z-axis value is 50uT and if I want to offset it to 0 then I can write 50uT to the OFFSET

Posted on July 22, 2017 at 08:34I am using LIS3MDL and is there any way to offset the interrupt threshold values by changing the Offset Registers? What I mean is suppose my surrounding environment z-axis value is 50uT and if I want to offset it to 0...

Reading data from LSM303AGR

Posted on June 22, 2017 at 15:50Hi, I'm new here and I am new at working on mems.I have a LPCXpresso1549 evaluation board and a Steval-MKI172v1 mems that implements a lsm303agr chip. I'm working on mbed platform and I need to read values from accele...

LSM9DS1 I2C address identification

Posted on June 22, 2017 at 09:56Hi,I am planning to use  LSM9DS1 9DoF sensor in our project. As per datasheet table #2, Least significant bit for I2C address is [SDO_   A/G or SDO_M ]= SA0.From this information & Table#19, I will be able to identify...