MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

VL53L1X: Is there only one kind of calibration (API), or there is a calibration that is made by ST for their dev. and breakout boards?

When I use the breakout board included in the dev kit, the precision is at most 2 mm, but when I use the VL53L1X soldered on one of my board, the precision is really different. Is there a particular calibration or setting that are input to the breako...

FLach by Associate
  • 1026 Views
  • 2 replies
  • 1 kudos

ISM330DLC : Noise Issue

Posted on July 16, 2018 at 08:55Hi,I am using ISM330DLC  accelerometer and gyroscope sensor.I have initialized the accelerometer & Gyroscope register and reading the respective X,Y,Z register and that is providing huge noise in gyroscope values. And...

shammi d by Associate II
  • 2720 Views
  • 7 replies
  • 0 kudos

Is there a way to detect overflow with LIS2MDL?

Posted on June 06, 2018 at 19:15GreetingsI am using the LIS2MDL to build a magnetic field sensor for the education market.  When the magnetic field being measured exceeds the maximum allowed value, I notice that the LIS2MDL returns unpredictable dat...

wild by Associate II
  • 1469 Views
  • 2 replies
  • 0 kudos

Resolved! A GPS module for STM32L1 MCU

Hi,I have a tracking project based on GPS.Could you please suggest me a GPS module that has a library for any STM32L1 MCU?Best regards.

LSM6DSL, LSM303AGR, LSM9DS1 temperature dependence

Posted on July 07, 2018 at 09:55I have conducted little research of temperature influence on accelerometr and gyroscope readings. The sensors were cooled to a negative temperature on celsius, and then heated under the IR lamp to approximately 50 deg...

0690X0000060C4lQAE.png 0690X0000060CFMQA2.png

VL53L1X: "Soldering the device on the customer board or adding a cover glass can introduce an offset in the ranging distance". Why does soldering the device on a board introduce an offset, and how much offset can it introduce?

A VL53L1X has been soldered on a board, and the result I get from ranging are offset by at least 15%. Can it be caused by the soldering itself? Will calibration remove the offset?

FLach by Associate
  • 799 Views
  • 0 replies
  • 1 kudos

DRDY_MAG interrupt on LSM303C?

Posted on June 28, 2018 at 04:13Can anyone tell me how to get a DRDY_MAG on the LSM303C?  Is that the correct interrupt to try and get for the magnetometer?  I'm trying to get mag data at about 10Hz and want an interrupt.  Nothing I have done has ca...