cancel
Showing results for 
Search instead for 
Did you mean: 

Pattern in FIFO_STATUS3 Register Does Not Update After Overrun Bit is Set

Audrey Hendon
Associate
Posted on June 29, 2018 at 19:58

 I 

am seeing some odd behavior when using the LSM6DSL sensor.

I have configured it to use the FIFO in continuous mode, enabled storing of gyro and accelerometer data, and enabled wakeups and the wakeup interrupt.The interrupts are working properly when a wakeup event has been detected, and I am able to pull samples out of the FIFO. However, the pattern registers(FIFO_STATUS3) do not seem to update once the overrun bit has been set. I am always seeing the same value for every pattern value that I read.

Do the FIFO_STATUS3 registers stop updating once the FIFO has overrun? Or is there a setup step that I may be missing?

#fifo-buffer #lsm6dsl
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Miroslav BATEK
ST Employee

Yes, the FIFO_STATUS3/4 registers (FIFO pattern) stop updating once the FIFO overrun.