MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LIS35DE Driver for Linux

Posted on July 16, 2018 at 09:02Hi All,I need device driver for LIS35DE MEMS motion sensor.CPU is I.MX6Q and linux platform kernel 4.4.0-130-generic.Could you give me a this driver?Thanks & BR,#lis35de

Field value 'recoil' upon metallic object proximity - LIS3MDL on X-NUCLEO-IKS01A1 and LSM303AGR on X-NUCLEO-IKS01A2

Base assumptions:1.    Testing equipment – X-NUCLEO-L053R8 base board with X-NUCLEO-IKS01A1 and X-NUCLEO-IKS01A2 expansion boards.2.    Magnetometer devices under consideration - LIS3MDL on X-NUCLEO-IKS01A1 and LSM303AGR on X-NUCLEO-IKS01A2.3.    Mag...

0690X0000060R1SQAU.jpg 0690X0000060R1XQAU.jpg 0690X0000060R1hQAE.jpg 0690X0000060R1mQAE.jpg
GGeor.4 by Associate II
  • 1044 Views
  • 1 replies
  • 0 kudos

I use LSM9DS1 with STM32L433 and get strange data.

I use LSM9DS1 with STM32L433 and get strange data.Initialization code:HAL_GPIO_WritePin(CS_A_G_GPIO_Port, CS_A_G_Pin, GPIO_PIN_RESET);   address = CTRL_REG4;   data = 0x38; //0b00111000   HAL_SPI_Transmit(&hspi1, &address, sizeof(address), 0x1000)...

0690X0000060QR1QAM.png

VL53L1X reflectance targets?

Prior to the forums being migrated, I saw a post linking to sites to obtain reflectance targets for calibrating and testing the VL53L1X or VL53L0X. I.e. Grey 17% N4.74, Grey 54%, and White 88% N9.5. I'm moving from breadboard development with the sat...

mdmottola by Associate II
  • 1152 Views
  • 1 replies
  • 0 kudos

How do I get the FP-NET-BLESTAR sample code to start sending all sensor data (acc, gyr and mag) from the STEVAL-STLCS01V1 sensor tiles?

It appears that the functionality is written into the code but I can't figure out how to get it to work. I am using the SW4STM32 IDE to build and compile and I know that in main.h there is #define ENABLE_MEMS 0 which can be changed to a 1 but the .h ...

LOver by Associate
  • 795 Views
  • 0 replies
  • 0 kudos

LSM9DS1 I2C address confusion

I have confusion about I2C address for magnetometer.As in the datasheet at page 11:SDO_M: I2C least significant bit of the device address (SA0) for the magnetometerBut in the table 20 page 30:See picture enclosedIt looks like the SDO_M pin is used fo...

NHuy.12 by Associate
  • 2795 Views
  • 3 replies
  • 0 kudos

Sparse LIS331 Datasheet(s)

Posted on July 12, 2018 at 08:16Dear all - especially STM developers,I recently integrated an LIS331HH sensor. It seams to be very nice sensor! But anyway while reading LIS331 Datasheet, I found that information required for proper MCU driver implem...

VL53L0x API data access inconsistency

The VL53L0X API (https://my.st.com/content/my_st_com/en/products/embedded-software/proximity-sensors-software/stsw-img005.license=1533144599665.html) requires definition of a platform-dependent structure of type VL53L0X_DevData_t. This structure must...

Using VL53L1X to detect ping pong balls on a table tennis board.

Hi all,I am designing an application which would tell me, if a ping pong ball lands on a particular area of a table or not. Below is a sketch that illustrates:Sensors would be placed on left side of the table, facing the other side as shown in the ab...

0690X0000060P00QAE.jpg
AHegd by Associate
  • 922 Views
  • 1 replies
  • 0 kudos