User Activity

Hi,I have a tracking project based on GPS.Could you please suggest me a GPS module that has a library for any STM32L1 MCU?Best regards.
Posted on March 13, 2018 at 23:07Hi,I have b-l072Z-LRWAN1 + SigFox SDR dongle. I added Node's ID to SENK (network emulator), then I loaded AT command and push button examples from X-CUBE-SFOX, and nothing worked. When I sent a frame, it seems that s...
Posted on January 31, 2018 at 19:15Hi,I have B-L072Z-LRWAN1 board from ST running I-CUBE-LRWAN software for LoRaWAN, and RHF0M301 gateway from RisingHF.I am testing a class C and I have an issue in downlink, here is the scenario: Node transmit an ...
Posted on October 03, 2017 at 20:40Hi,I am trying to write data to a text. The code is shown below. I am using STM32L152D board with Keil V5.When I exceute the code, nothing works at all.#include <stdio.h>main(){FILE *fp;fp = fopen('/tmp/test.txt', ...
Posted on September 23, 2017 at 05:45I am using LIS3MDL sensor and I do not understand the sensitivity which its unit is LSB/Gauss.  In x-cube-mems1 library, the following is calculated:&sharpdefine LIS3MDL_MAG_SENSITIVITY_FOR_FS_4G    0.14 /**< Sen...
Kudos from