MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LSM9DS1 I2C address confusion

I have confusion about I2C address for magnetometer.As in the datasheet at page 11:SDO_M: I2C least significant bit of the device address (SA0) for the magnetometerBut in the table 20 page 30:See picture enclosedIt looks like the SDO_M pin is used fo...

NHuy.12 by Associate
  • 2895 Views
  • 3 replies
  • 0 kudos

Sparse LIS331 Datasheet(s)

Posted on July 12, 2018 at 08:16Dear all - especially STM developers,I recently integrated an LIS331HH sensor. It seams to be very nice sensor! But anyway while reading LIS331 Datasheet, I found that information required for proper MCU driver implem...

VL53L0x API data access inconsistency

The VL53L0X API (https://my.st.com/content/my_st_com/en/products/embedded-software/proximity-sensors-software/stsw-img005.license=1533144599665.html) requires definition of a platform-dependent structure of type VL53L0X_DevData_t. This structure must...

Using VL53L1X to detect ping pong balls on a table tennis board.

Hi all,I am designing an application which would tell me, if a ping pong ball lands on a particular area of a table or not. Below is a sketch that illustrates:Sensors would be placed on left side of the table, facing the other side as shown in the ab...

0690X0000060P00QAE.jpg
AHegd by Associate
  • 944 Views
  • 1 replies
  • 0 kudos

VL53L1X: Is there only one kind of calibration (API), or there is a calibration that is made by ST for their dev. and breakout boards?

When I use the breakout board included in the dev kit, the precision is at most 2 mm, but when I use the VL53L1X soldered on one of my board, the precision is really different. Is there a particular calibration or setting that are input to the breako...

FLach by Associate
  • 1049 Views
  • 2 replies
  • 1 kudos

ISM330DLC : Noise Issue

Posted on July 16, 2018 at 08:55Hi,I am using ISM330DLC  accelerometer and gyroscope sensor.I have initialized the accelerometer & Gyroscope register and reading the respective X,Y,Z register and that is providing huge noise in gyroscope values. And...

shammi d by Associate II
  • 2817 Views
  • 7 replies
  • 0 kudos

Is there a way to detect overflow with LIS2MDL?

Posted on June 06, 2018 at 19:15GreetingsI am using the LIS2MDL to build a magnetic field sensor for the education market.  When the magnetic field being measured exceeds the maximum allowed value, I notice that the LIS2MDL returns unpredictable dat...

wild by Associate II
  • 1517 Views
  • 2 replies
  • 0 kudos