MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

iis328dq accelerometer data frequency

hai , iam using ii2328dq for reading the accelerometer values so here from sensor i got continues data how to know that frequency of data and could you pkease tell me how tocontrol that sensor data frequency.

cmoul by Associate
  • 771 Views
  • 1 replies
  • 0 kudos

How to program firmware and use Unicleo-GUI

I have recently purchased an STM32F767ZIT6 Nucleo kit, as well as an X-Nucleo-IKS01A2 MEMS expansion board. I installed Unicleo-GUI, and downloaded the X-CUBE-MEMS1 software. I can't figure out how to get firmware to run on the board though. I dro...

BDoon by Associate II
  • 1147 Views
  • 1 replies
  • 1 kudos

LIS35DE Driver for Linux

Posted on July 16, 2018 at 09:02Hi All,I need device driver for LIS35DE MEMS motion sensor.CPU is I.MX6Q and linux platform kernel 4.4.0-130-generic.Could you give me a this driver?Thanks & BR,#lis35de

Field value 'recoil' upon metallic object proximity - LIS3MDL on X-NUCLEO-IKS01A1 and LSM303AGR on X-NUCLEO-IKS01A2

Base assumptions:1.    Testing equipment – X-NUCLEO-L053R8 base board with X-NUCLEO-IKS01A1 and X-NUCLEO-IKS01A2 expansion boards.2.    Magnetometer devices under consideration - LIS3MDL on X-NUCLEO-IKS01A1 and LSM303AGR on X-NUCLEO-IKS01A2.3.    Mag...

0690X0000060R1SQAU.jpg 0690X0000060R1XQAU.jpg 0690X0000060R1hQAE.jpg 0690X0000060R1mQAE.jpg
GGeor.4 by Associate II
  • 1081 Views
  • 1 replies
  • 0 kudos

I use LSM9DS1 with STM32L433 and get strange data.

I use LSM9DS1 with STM32L433 and get strange data.Initialization code:HAL_GPIO_WritePin(CS_A_G_GPIO_Port, CS_A_G_Pin, GPIO_PIN_RESET);   address = CTRL_REG4;   data = 0x38; //0b00111000   HAL_SPI_Transmit(&hspi1, &address, sizeof(address), 0x1000)...

0690X0000060QR1QAM.png

VL53L1X reflectance targets?

Prior to the forums being migrated, I saw a post linking to sites to obtain reflectance targets for calibrating and testing the VL53L1X or VL53L0X. I.e. Grey 17% N4.74, Grey 54%, and White 88% N9.5. I'm moving from breadboard development with the sat...

mdmottola by Associate II
  • 1188 Views
  • 1 replies
  • 0 kudos