MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! A GPS module for STM32L1 MCU

Hi,I have a tracking project based on GPS.Could you please suggest me a GPS module that has a library for any STM32L1 MCU?Best regards.

LSM6DSL, LSM303AGR, LSM9DS1 temperature dependence

Posted on July 07, 2018 at 09:55I have conducted little research of temperature influence on accelerometr and gyroscope readings. The sensors were cooled to a negative temperature on celsius, and then heated under the IR lamp to approximately 50 deg...

0690X0000060C4lQAE.png 0690X0000060CFMQA2.png

VL53L1X: "Soldering the device on the customer board or adding a cover glass can introduce an offset in the ranging distance". Why does soldering the device on a board introduce an offset, and how much offset can it introduce?

A VL53L1X has been soldered on a board, and the result I get from ranging are offset by at least 15%. Can it be caused by the soldering itself? Will calibration remove the offset?

FLach by Associate
  • 826 Views
  • 0 replies
  • 1 kudos

DRDY_MAG interrupt on LSM303C?

Posted on June 28, 2018 at 04:13Can anyone tell me how to get a DRDY_MAG on the LSM303C?  Is that the correct interrupt to try and get for the magnetometer?  I'm trying to get mag data at about 10Hz and want an interrupt.  Nothing I have done has ca...

marking LSM9DS0TR

Posted on July 16, 2018 at 10:48Hello I am very need you help. For identification I am very need know how stands for marking LSM9DS0TR:first line: 9S0second line: 2716third line: P7GAU#marking-lsm9ds0tr

VL53L1X device address storage

Posted on July 01, 2018 at 10:43Can anybody tell me if the VL53L1X device address is stored in volatile or non-volatile memory? I have multiple sensors in application and i don't want to have reset/shudown lines for every single one of them just for...