Posted on February 26, 2018 at 09:17 Hi, I'm trying to read out the accelerator values using STEVAL-STLKT01V1, on iOS. Is there any possibility to set the sample rate of the sensor?
Note: this post was migrated and contained many threaded c...
Posted on February 28, 2018 at 22:39 Ok, in that case the 104 Hz you were mentioning earlier refers to which thing - ODR or Data Reading frequency? Also could you pls point me to the Sources of ALLMEMS1 as well as FW update instructions?
Posted on February 27, 2018 at 19:31Hi, I have finally attached the sensor. Could you pls. explain the following results:First number is the 'receiving timestamp' on iOS App, second is the Node Timestamp, third the value (Accelerator Z).I assume the...
Posted on February 26, 2018 at 17:20Ok, so do I get it right that the sample rate will be automatically defined by the maximum possible hardware rate ?
Posted on February 26, 2018 at 10:00When I connect to the sensor using ST App the sensor is found as BM2V220. I do not see any other possibility to read out the FW version. I've got sensors from my customer for whom I should write an iOS app so I do...