MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STEVAL-BFA001V1B wrong cable description

I wanted to try the STEVAL-IDP005V1 from STEVAL-BFA001V1B,I followed the description given in UM2438and nothing worked,Finally I realized that the cable description is wrong (or may be I've got a bad cable),the ground is on white, not on blue wire

MMade.1 by Associate II
  • 2352 Views
  • 5 replies
  • 0 kudos

Using LIS2DH on a SPI bus with many devices

It seems that its CS is inactive, the LIS will assume that it should be in I2C mode.But if I have multiple devices on the SPI bus, then I want to be able to disable I2C mode altogether.Our board has exactly this setup and it seems that whenever I ena...

LPS27HHW - Application note how to mount on housing

Hello,I'm looking for any available douments/application notes on how to mount the sensor on a device housing. For example I would like to know what is the suggest o-ring, is it safe to expose the sensor opening to the external world or it needs some...

Resolved! LIS2DE12 coherency in bypass mode

Hi,I am using an LIS2DE12 in I2c mode.  During setup, my code:- wrote 0 to CTRL_REG4 (BDU=0, FS=00, ST=00, and SIM=0)- wrote 0 to CTRL_REG2 (no high-pass filtering)- wrote 0 to CTRL_REG5 (disable FIFO)- wrote 0 to FIFO_CTRL_REG (selects Bypass mode)-...

ILPS22QS pressure sensor holding SCL high

We have a ILPS22QS pressure sensor.We are getting an occasional i2c error.On investigation it seems the ILPS22QS sensor is holding the SCL line high during a pressure reading.I have read through the datasheet and see no functionality that would allow...

o0p3Ujx unnamed(1).jpg
mattc by Associate
  • 692 Views
  • 0 replies
  • 0 kudos

Resolved! LSM6DSOX MLC

Hi Team,  We are working with the LSM6DSOX sensor and integrating it with two different MCUs: nRF5340 and ATSAMD51, using the I2C communication protocol. We have been able to successfully read the device ID, accelerometer data, and gyroscope data. Ad...