MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LSM6DS3, any reason not to run it on 2.5VDC supply?

We're designing the LSM6DS3 into an existing product that already uses a 2V5 supply rail. The LSM6DS3's spec sheet says that running it at 2V5 is well within spec, but all of the examples refer to a 1V8 supply. Is there any reason that a 2V5 supply i...

Using STEVAL-MKI109V3 with Windows 10

Hi,I struggle to use the STEVAL-MKI109V3 board with Windows 10. The VCP serial port is detected, but the OS is unable to attach the right driver (a yellow exclamation mark is shown in the Device Explorer). Other STM32 boards with USB CDC do work fine...

how to simulate Sent protocol ?

Hello everybody,I wanted to simulate the Sent_Protocol with a STM32 µC or simulate it as if I had a sensor. and present this with oscilloscope. Now the signal should be like a normal PWM Signal look like. I really do not know how to generate this par...

Samuel1 by Associate III
  • 2275 Views
  • 0 replies
  • 0 kudos

L3GD20H can't set Low_ODR bit

Hi everyone,I am using a L3GD20H gyro on a custom board. I am successfully talking to it and have been able to set the following registers to values:CTRL1_reg: 0x0F (power enabled, all axes enabled)CTRL3_reg: 0x08 (INT2 set for data ready signal)CTRL...

MMacL.12 by Associate
  • 1815 Views
  • 3 replies
  • 0 kudos