cancel
Showing results for 
Search instead for 
Did you mean: 

Using STEVAL-MKI109V3 with Windows 10

Christophe Thil
Associate

Hi,

I struggle to use the STEVAL-MKI109V3 board with Windows 10. The VCP serial port is detected, but the OS is unable to attach the right driver (a yellow exclamation mark is shown in the Device Explorer). Other STM32 boards with USB CDC do work fine.

I tried to upgrade the firmware to version 2.40.1 (included with Unico), which seemed to be succesful.

I'd be very happy for any hints on how to operate the eval kit with Win10. Thanks.

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
Jacek Pieczaba
Associate II

I have the same issue... If you advice us what we can do in order to make it works under Windows 10 it will be great. Thank you

AvaTar
Lead

You could try to play with Windows options, especially compatibility settings.

VDhan
Associate II

Hello all,

I was also facing the same issue, rather than updating the driver from device manager I resolved this issue by installing VCP_V1.5.0_Setup_W8_x64_64bits from installation folder: MEMS_Demonstration_Kit_SW_package_v8_0_WINDOWS-> Driver->STM32_vcp.

Try this let me know if it works for you.

Thank you

D.Vishnu

Thank you your suggestion works very good. Have a great day​