MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

FIFO sampling of LSM6DSL and "missing" samples

I have programmed the LSM6DSL to a sample rate ODR of 26Hz, and set the FIFO ODR to 26Hz (I've also tried much higher FIFO ODR rates). I am only sampling the accelerometer. Every second, I read the FIFO and am expecting to find 26 samples. Or, at ...

JBenn by Associate
  • 1580 Views
  • 1 replies
  • 0 kudos

Connecting sensor Tile with unicleo gui on bluetooth

Hi,I'm in charge to develop application for vibration monitoring with sensorTile.but i'm not able to connect the sensor tile with bluetooth on unicleo gui. Despite all my work, update and any thing i can do, unicleo dont want to detect the sensor. I'...

0690X0000087XPUQA2.jpg

HTS221 does it works or does it only have manufacturing defects?

Hello everyone, i apologize for my bad English. I use HTS221 in one of my products, i tested it on evaluation-board and it worked perfectly so i decided to use it in production and I already produced 400 PCB in 3 years. But it doesn't work! the tempe...

AAssi by Associate II
  • 891 Views
  • 0 replies
  • 0 kudos

LIS3DH wrong out value +-16g

Posted on September 28, 2016 at 12:35Hi,LIS3DH, I don't move it. Sampling rate 400 Hz, CTRL_REG2=0.+-2g full scale : (0g;0g;1g) out value+-4g full scale : (0g;0g;1g) out value+-8g full scale : (0g;0g;1g) out value+-16g full scale : (0g;0g;0,67g) out...

My Test Code to Initialize LSM6DSM Gryo to Observe Pulses on INT1 coming from the Device does not work - Any Suggestions to Fix?

Here is my test code, that I single-step to observe the reg_status first, then write what I think should start the device, but I see nothing on INT1. Each reg_status read show the correct data (same as what I am writing):   reg_status = ReadReg(LSM6D...

design23 by Associate II
  • 821 Views
  • 0 replies
  • 0 kudos

Resolved! Tilt angle sensor

We are looking for a sensor that can identify tilt angle with respect to gravity. I have been looking around at 3-axis accelerometers but cannot be sure if these will work as a tilt angle sensor. Please advise.NOTE: This question and answer originate...

Unable to find Test code for the LSM9S1 SPI Driver code

Hi, I am trying to integrate the STMems_Linux_Input_drivers for the LSM9DS1 into the custom kernel written by one of team members. However, I am not able to find the sample program or test program to test the drivers. My SOC is Texas Instrument TSM57...

NAhme.5 by Associate
  • 744 Views
  • 0 replies
  • 0 kudos

LSM303AGR CTRL_REG4 FS[1:0] Full Scale Selection is reversed?

Hi,Based from the LSM303AGR CTRL_REG4 FS[1:0} Full Scale Selection are (00: ±2g; 01: ±4g; 10: ±8g; 11: ±16g). I tried all settings and it is reversed. So, setting 00 is +-16g. So is this an error in the datasheet?Regards,Markel

MRobr by Associate III
  • 666 Views
  • 0 replies
  • 0 kudos