MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to change working modes of VL53l0X at runtime

I am using ST s API(VL53L0X TOF Sensor) and i have a doubt regarding the change in ranging modes at run time,For my application i want the sensor to work in HIGH ACCURACY mode first and after a time it has to work on FAST MODE and again back to HIGH ...

sp ra by Associate
  • 4088 Views
  • 1 replies
  • 0 kudos

Resolved! LSM6DSOX And STM32cube

Hi,​I am using LSM6DSOX and ProfiMEMS​ board . I have created my modelm based on WEKA(decision tree) and I tested it in Unico v.8 and it worked.Now the question is how can I use my final model(the model which I loaded in MLC)​ in STM32cube? How is th...

spark by Associate II
  • 2229 Views
  • 3 replies
  • 0 kudos

Is it possible to access data of only one SPAD of the VL53L1X ?

Hi everyone,For a project I need to know if i can access the data of only one SPAD and not the data of the entire array.I need to detect with precision the position of some objects and I'm wondering if that is possible with the VL53L1X. My idea is (i...

MF by Associate
  • 1419 Views
  • 2 replies
  • 0 kudos

Accelerometer with higher operating temperature range?

Hi,I am using the accelerometer IIS2DLPTR and i saw in the datasheet that the maximum operation temperature is 85°C. Is there an accelerometer that has the same features that the one I am using but that has a higher maximum operation temperature?Best...

VGuer by Associate II
  • 2090 Views
  • 4 replies
  • 0 kudos

MotionAW does not leave MAW_STATIONARY

Hi,​Im trying to evaluate MotionAW on a BlueCoin dev kit. After a few seconds MotionAW_Update returns AMW_STATIONARY (before that it returns MAW_NOACTIVITY), and after that the activity doesnt seem to change. What am I doing wrong?For all I can see t...

HSmed by Associate
  • 818 Views
  • 0 replies
  • 0 kudos

Resolved! VL53L1X RangeStatus No Update problem

Hi!I want use an VL53L1X sensor for our project. I "ported" to original ST api to TI chip and TIRTOS. But I cant measure any distance. Now I just want to try the sensor, so I using "polling" method. But when I call a GetMeasurementDataReady function...

RSzil by Associate
  • 1998 Views
  • 2 replies
  • 0 kudos