User Activity

Hi,I am using the accelerometer IIS2DLPTR and i saw in the datasheet that the maximum operation temperature is 85°C. Is there an accelerometer that has the same features that the one I am using but that has a higher maximum operation temperature?Best...
Hi,In the company where I work we are developing hardware and we are already evaluating the LIS3DH in order to put it in our hardware devices. However we have noticed that the LIS3DH is obsolete but there is the LIS3DHTR which is the same product but...
I have a LIS3DH sensor and Unico 7 in my computer and I am using the evaluation board MKI109V3. The thing is that I want to save the temperature data (measured by the Embedded Temperature sensor inside the LIS3DH) in a log file and with Unico this is...
Hi,I installed the Unico 7.0.0, the driver for the MKI109V3 and the DfuSe application contained in the MKI109V3 package. I wanted to upload the firmware on the board as the instruction manual UM2116 says. Therefore I changed the board to DFU mode and...