MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LIS3MDL for detecting car occupancy in parking space

Hi I am considering LIS3MDL to detect the presence of car in parking space by measuring the change in magnetic field. Has anyone worked on this LIS3MDL for similar application? Would you please share your experience / comments?ThanksSilas

Regarding the Configuration of the STEVAL MKI175v1(LIS2DE12)

I am using this Accelerometer and in the datasheet it is mentioned that the Bit 4(LPC) in CTRL_REG1 should set for the Proper operation of the Device,but when i set that device the Sensor ,i am not getting any values in that, i want to know ,is it re...

NMuth by Associate II
  • 871 Views
  • 1 replies
  • 0 kudos

LIS3DH ADC calibration

LIS3DH is configured with ADC enabled, and temperature disabled.When the same voltage is applied to all the 3 ADC inputs, the ADC reading on the first 2 inputs are matching and in line with the expected readings. However, the 3rd input show a constan...

MArgi by Associate II
  • 1268 Views
  • 1 replies
  • 0 kudos

I'm looking for an equivalent to the LOPS33W sea water compatible pressure sensor, but with 2 and 4 ATM (and possibly higher) absolute full scale ranges.

The digital IO of pressure and temperature is nice, but we can also use an analog output. The digital is good for a new high volume project, but we need an analog output for a current application. Small size and low power requirements are also impo...

WBors by Associate
  • 800 Views
  • 2 replies
  • 0 kudos

Need reference schematic for #LSM6DSOX.

Hello,I use #LSM6DSOX​ in our product development. i need to this device configure with nRF51822 or other MCU.Could you please share reference schematic for same.Please, It would be helpful in our product development.Thank you.

cc007 by Associate
  • 1097 Views
  • 1 replies
  • 1 kudos

How to solve link error on blue-coin source(STEVAL-BCNKT01V1)?

I have to change MCU from STM32F466 to STM32F722 in the STEVAL-BCNKT01V1 sample code and build by the uVision(KEIL). I was build and test on the STM32F722 board using by IAR workbench.(Working properly)And I had converted to KEIL and build using by u...

HKim.18 by Associate
  • 1223 Views
  • 1 replies
  • 0 kudos

Resolved! Slow reading of AIS328DQ output

My question concerns the ZYXDA status bit of STATUS_REG (27h)If I'm reading data out at a significantly lower rate (e.g. 25Hz) than the device is internally generating data (100Hz) is there any need to monitor this status bit?Asked another way, Can I...

www.st.com

AWS-Conn#11: the SW platforms - the STBLESensor app (old BlueMS app)STBLESensor is the general application, available for Android and iOS, for testing ST sensors with your smartphone and for logging the data exported by a BLE device using the BlueST ...

0690X000008BNugQAG.jpg

LIS3MDL: Stops converting

I am using the LIS3MDL in continuous conversion mode - high speed at 1KHz. Intermittently it stops converting, the data ready line stays low. I can do a soft reset and the part does not recover. The only way I can recover the part is to power cycle i...