MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX X-NUCLEO-IKS01A2 X-CUBE-MEMS1

I Refered to Page 25 ,7.1 of the Document and Used of MEMS Library without sample applications for XNUCLEO-IKS01A2 with NUCLEO-L4R5ZI. in the platform setting there is no BSP_BUS_DRIVER ,i2c。another problem is that BSP_USART has no solution. Who kno...

0690X000008wDNFQA2.png 0690X000008wDNKQA2.png
Fgg by Associate II
  • 827 Views
  • 0 replies
  • 0 kudos

Use MotionFX with Keil

Hi to all,I'm doing a Keil project using the MotionFX library contained in the xCube-mems1 v6.0.1, the project run a STM32F407ZG.I've enabled the CRC clock, I've added the library "MotionFX_CM4F_wc16_ot.a", I've enabled the FPU unit.I can build the p...

Mezzo by Associate II
  • 1829 Views
  • 5 replies
  • 0 kudos

Issue with LIS3DSH machine state

Hi everyone,I'm trying to use the machine states of the LIS3DSH (on a STEVAL_MK109V3 in the ST unico utility) to implement a mechanism to provide an interrupt when a series of movements happen in a defined time slot, to trigger a trip start event, an...

CMugi by Associate
  • 1718 Views
  • 1 replies
  • 0 kudos

Some issue for the raw data of X axis in LIS3DH.

Dear All: I have a project to read LIS3DH data and use STM32F745 MCU to access 3 Axis of LIS3DH data. After initial LIS3DH control register(CTRL1_REG=0x47 /*set ODR as 50 Hz and enable Ax Ay Az....*/ and CTRL4_REG=0x88 /*enable block data update(BDU)...

HTS221 inconsistency

Hello All,Good day!I got three boards placed close to each other but the humidity readings on three boards varies. Say, 1 board has a humidity reading of ~50 %, the other has ~60% and the last one has ~70 %. I'm not testing it on a closed environment...

ERefo by Associate II
  • 2791 Views
  • 3 replies
  • 0 kudos

How to choose the accelerometer recording frequency.

I have instaled the "ST BLE Sensor" on my smartphone and made some data collecting using accelerometer sensor. I have seen on the APP presentation that is possible to choose the frequency but I didn't find this option in the APP. I am seding a image...

0690X000008AOt5QAG.png
GTell by Associate II
  • 3546 Views
  • 9 replies
  • 0 kudos

LSM303C magnetometer automatic calibration not working in Android

I use a LSM303C magnetometer sensor on an Android platform.Sensor works fine, however automatic calibration (hard and soft iron) does not work. I checked it using an Android app displaying magnetic field vector in 2D, for both calibrated and uncali...

0690X000008BfSCQA0.png 0690X000008BfVaQAK.png
IGEHI by Associate
  • 2796 Views
  • 2 replies
  • 0 kudos