MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

L3GD20H Motion Sensor

Hello,I am using the ​L3GD20H Motion Sensor for flight application and I need to compensate for temperature variation. There is a registry that I can read that provides a temperature value. Could you tell me what this value means and what it is refer...

PCote by Associate
  • 1342 Views
  • 3 replies
  • 0 kudos

Twait: LSM303CTR Why is there a Twait for IO pins and Vdd?

In the datasheet Twait was added to inform us to delay between powering up Vdd_IO and Vdd. However, the Twait timing says that there should be 0-10 mS wait period between Vdd-IO and Vdd. After waiting 0.1 - 100 ms Rise Time for Vdd-IO. What is the...

TSing.13 by Associate
  • 933 Views
  • 1 replies
  • 0 kudos

Send MEMS-Mic-Audio to PC-Host

Hi, I try to connect a Nucleo-144-Board to Audacity. The Project is based on CubeMx5.2/STM32Cube_FW_L4_V1.14.0. I've read (successfully) in a Mems-Mic via SAI1/DMA2. The USB-Audio-Device is shown in the Device-Manager and seems to be OK. I've read th...

TTimm by Associate II
  • 1516 Views
  • 2 replies
  • 0 kudos

State Machine and stack size ?

Dear Members,I have a state machine but it seems that it stuck in one state,Is it related with stack size ?It's stuck on "case PULSE_IDLE" no matter the value of sensor_value,The code :switch(currentPulseDetectorState) { case PULSE_IDLE: ...

LIS3MDL Magnetometer Calibration

Hi, From what I've been told, the LIS3MDL magnetometers self-calibrate upon turning on. I have taken some readings from 3 different LIS3MDL's and plotted the values in a similar way to the beginning of this tutorial: https://thecavepearlproject.org/2...

0690X000008aEipQAE.png 0690X000008aEj4QAE.png 0690X000008aEklQAE.png 0690X000008aEkqQAE.png